SUG_Wiser_China_WSE-06

Creating a Moment using the freelocate (E-mode)

Perform this task to create a Moment that can be triggered by pressing a button on the Wiser AvatarOn Freelocate.

The devices to be used in the Moment must first be added to the E-mode system.

  1. Operate the local control on each device to the required level or position to create the Moment:
    1. Switches: Switch lights On/Off as desired.
    2. Dimmers: Operate the dimmer to full brightness, then dim the light down to the desired level.
    3. Curtain switches: Operate the curtains to fully-open or fully-closed only.
  2. The devices used in the Moment work in toggle control. For example if the current status in a group of light switches is Off, when a user triggers the Moment, the status of the group devices will change to On.
  3. Set the freelocate to programming mode. (See Setting programming mode on a Wiser AvatarOn Freelocate.)
  4. Short press the local control button on each device used in the Moment.
    The local control backlight on each device starts flashing.
  5. Long press (more than 2 seconds) the freelocate button that will be used to trigger the Moment.

The programming LEDs on each device and the freelocate flash green 5 times to confirm that the Moment settings have been assigned to the freelocate button.

NOTE: The new assignment overrides any Moment settings previously assigned to the freelocate button.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.