SUG_Wiser_China_WSE-06

Installing and testing devices

Install and test light switches, dimmers, sensors and other devices before using the app to configure the Wiser system.
  1. Follow the installation instructions supplied with each device. See Supported Wiser devices.
  2. Ensure that the batteries in battery-powered devices are installed and in good condition. Refer to the device instructions for low battery indications.
  3. When installing Wiser multifunction interfaces, connect thermostats that are compatible with the device. See Compatible thermostats for the Wiser Multifunction Interface.
    NOTE: See Selecting a location for the Wiser Hub or Basic Hub for information regarding location selection for Hub.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.