SUG_Wiser_China_WSE-06

Setting up an E-mode system

There are 4 tasks to set up an E-mode system.

Task

Reference

Create a Zigbee network for the E-mode system.

See Creating the network for E-mode.

Add devices to the E-mode system.

See Adding devices to the E-mode system.

Assign device control operations to the buttons on a freelocate for remote control.

See Assigning device control operations to a freelocate button (E-mode).

NOTE: Before performing this task, the freelocate must be set to programming mode. (See Setting programming mode on a Wiser AvatarOn Freelocate.)

Create Moments using the freelocate,

See Creating a Moment using the freelocate (E-mode).

NOTE: Before performing this task, the freelocate must be set to programming mode. (See Setting programming mode on a Wiser AvatarOn Freelocate.)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.