SUG_Wiser_China_WSE-06

Creating the network for E-mode

Use a compatible Wiser AvatarOn device to create a Zigbee network for the E-mode system.
IMPORTANT: When setting up more than one E-mode system for the home. Only create one network at a time. If another network is being created when you perform this task, the device you use will join that network instead of creating a new one.
  1. Select a compatible device to create the network. (See Supported devices for E-mode set-up.)
    NOTE: Only light switches, dimmers and curtain switches can be used. The freelocate is not capable of creating a network.
  2. Locate the Setup/Reset button on the device.
  3. Short press the Setup/Reset button 3 times.

The programming indicator LED on the device displays solid green and the network is created.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.