SUG_Wiser_China_WSE-06

Assigning device control operations to a freelocate button (E-mode)

Perform this task so that users can remotely operate the controls on Wiser AvatarOn switches/dimmers, or Wiser AvatarOn curtain switches, using the buttons on a Wiser AvatarOn Freelocate.
TIP: Wiser AvatarOn Light Switches and Dimmers are operated differently to Wiser AvatarOn Curtain Switches. Assign curtain switch controls to a different freelocate button than that used for light switches/dimmers.
  1. Select a Wiser AvatarOn device and short press the local control button to be assigned.
    The local control backlight starts flashing.
  2. To remotely control multiple device buttons from one freelocate button: Select more devices in the E-mode system and press their local control buttons.
  3. Short press the freelocate button that will operate the selected device controls.

The backlight on each selected local control, and the freelocate programming LED, flashes 5 times.

NOTE: The new assignments override any device controls previously assigned to the freelocate button.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.