SUG_Wiser_China_WSE-06

LED Behavior

Device

Status

LED indication

Duration

Wiser Basic Hub

Switch On/ Indication that the Basic Hub is working

During system booting, both Zigbee and Network LEDs are On.

After system booted, Zigbee LED is On, Network LED is Off when no network connection/ Network LED is On when there is network connection.

System booting duration is approx. 40 seconds.

Connected to the Wi-Fi or Ethernet

Network LED is always On

While connected to the Wi-Fi or Ethernet

The Basic Hub is in AP mode

Network LED blinks

10 mins approx.

The zigbee network formed

Zigbee LED is On

While connected to the power cable

Trigger the Zigbee commissioning process

Zigbee LED blinks

254 seconds approx.

In installation mode

Zigbee and Network LED blinks

Both LEDs will stop blinking once the commissioning is completed.

Level 1 reset

Zigbee and Network LED blinks

Once

Level 2 reset

Zigbee and Network LED blinks

3 times
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.