SUG_Wiser_China_WSE-06

Supported devices for E-mode set-up

Selected devices are capable of creating a Zigbee network for E-mode.

Supported devices include the following:

  • Wiser AvatarOn 1G Switch
  • Wiser AvatarOn 2G Switch
  • Wiser AvatarOn 3G Switch
  • Wiser AvatarOn 1G Curtain Switch
  • Wiser AvatarOn 2G Curtain Switch
  • Wiser AvatarOn 1G Dimmer
  • Wiser AvatarOn 2G Dimmer.
  • AvatarOn T switch 1G Switch
  • AvatarOn T switch 2G Switch
  • AvatarOn T switch 3G Switch
  • AvatarOn T 1G Curtain Switch
  • AvatarOn T 2G Curtain Switch
  • AvatarOn T1G Curtain Switch
  • AvatarOn T 2G Curtain Switch
  • AvatarOn T 6K Freelocate
  • AvatarOn T 4K Freelocate
  • AvatarOn T 5P Switch sockets
NOTE: While a Wiser AvatarOn Freelocate can be used in an E-mode system, it cannot create the required network.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.