SUG_Wiser_China_WSE-06

Wiser Motion Sensor

Symptom

Possible cause

Solution

The Motion Sensor has stopped reporting occupancy status, but is otherwise operating normally.

The Motion Sensor may be undergoing an over-the-air (OTA) firmware update.

Wait for the firmware update to complete and then check that the motion sensor is reporting occupancy status.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.