SUG_Wiser_China_WSE-06

Moment (E-Mode)

The effect created by adjusting the settings on one or more Wiser AvatarOn devices such as lighting switches, curtain switches and dimmers. For example, create a relaxed mood for the evening by closing the curtains and dimming the lights to half-brightness. Multiple device settings can be assigned to a Wiser AvatarOn Freelocate to trigger the Moment at any time with the push of a button.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.