SUG_Wiser_China_WSE-06

Dimmers

Wiser AvatarOn 1G Dimmer

Wiser AvatarOn 2G Dimmer

AvatarOn T 1G/2G Dimmer

Controls the lighting level in a room, or automatically set lighting to a desired level in response to a specified condition or event.

AvatarOn 1G Dimmer

AvatarOn 2G Dimmer

AvatarOn T 1G/2G Dimmer

Wiser 1 Gang Micro Module Dimmer

Converts compatible momentary switches into smart dimmers. Connect up to 10 compatible momentary switches .

NOTE: Momentary switches must be certified for use in 220–240 V AC applications.

Instruction Sheet (PDF)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.