SUG_Wiser_China_WSE-06

Programming the keys on a freelocate

Assign a Moment to a key on the freelocate remote controller .

You can add an existing Moment to a freelocate key, or create a Moment as part of the programming task. You can assign only one Moment to a key.

If you choose to create a new Moment as part of this task:

  • The creation process is best described in Creating a Moment.

  • The new Moment will be verified when complete. You then assign the newly created Moment to a freelocate key.

  1. In the app, select a freelocate and open the device page.

  2. (See A): Tap and hold one of the keys displayed on the page.
    (For 2K freelocates , only 2 keys are displayed.)
  3. (See B): In the Icon Moment Settings page, tap Icons and choose an icon to display on the key.
  4. (See C): Tap Select Moment Mode , then perform step 5, 6 or 7 only.
  5. (Optional) Add a cloud-based Moment (can only be used when wiser hub is present and the system is connected to the internet. This is the most flexible option because you can control everything including IR, Multifultion Interface and WiFi devices):
    1. (See D) Tap Moment with Multifunction Interface & IR Convertor.
    2. Either select an existing Moment displayed on the page, or tap Add Moment to create a new one.
    3. Go to step 8.
  6. (Optional) Add a local Moment (can be used without Internet once configured. This option provides control for moments which only contain Zigbee devices.):
    1. (See E) Tap Moment without Multifunction Interface & IR Convertor.
    2. Either select an existing Moment or tap Add Moment to create a new one.
    3. Go to step 8.
  7. (Optional) Add a Moment containing a device group (can be used without Wiser Hub and without Internet once configured. Zigbee group devices are controlled using freelocate switch.)
    1. (See F) Tap Group.
    2. In the Group Setting page, tap Add Moment and create a Moment containing a group of devices.

      (For example, add all the lights in one room or area to be operated from the freelocate switch.)

      TIP:
      1. Only group devices that operate in a similar way. For example, lighting only, or curtain control only.

      2. The group devices controlled by freelocate switch operated in toggle control. For example, if the current status in a group of light switches is Off, when a user press the pre-configured key on freelocate switch, the status of the group devices changes to On.

    3. Go to step 8.
  8. After selecting the Moment to assign to the freelocate key, tap Complete to finish the task.
    TIP: You may be prompted to wake battery-operated devices before the task can be completed.
    NOTE:

    You can wake up battery devices:

    • In general, short press program button once.

    • For the devices which have local push button such as AvatarOn freelocate switch, it is okay to press the push button.

    • For motion sensor battery devices, wave hand in front of the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.