SUG_Wiser_China_WSE-06

Adding the Basic Hub to the Home

Use the app to add the Basic Hub to a Home.
  1. Log in to the app.
  2. (See A) Select the Home to which the Basic Hub will be added.
  3. (See B) In the Home page, tap the + icon.

  4. In the Add Device page, do the following:
    1. Tap Auto Scan.
    2. If prompted, follow any instructions displayed on the page.
    3. Tap Start scanning.
    4. Tap the hub device name displayed on the app page and follow the steps in the app.
Once the process is complete, the Basic Hub is displayed as a device on the Home page.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.