SUG_Wiser_China_WSE-06

Resetting the Basic Hub

Delete existing settings from a Hub for commissioning or to remove a Hub from the system. It may also be necessary to restore the Hub .
  • For resetting the Ethernet and Wi-Fi settings, long press the reset button between 5 s to 15 s.

  • For resetting the device to factory default mode, long press the reset button for more than 15 s.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.