SUG_Wiser_China_WSE-06

IP Camera Indoor

The IP camera is connected to the system via the network router. To pair the camera with the app, see Pairing the device and follow the steps to add the device from the home page. Therefore, commissioning of the hub is not required before pairing.

After the device is added, follow the instructions in the app to complete the pairing process.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.