SUG_Wiser_China_WSE-06

System requirements

To use the app, your mobile phone/tablet must support following operating systems and versions.

Supported operating systems for mobile phone:

  • Android™ OS version 7 and above
  • Apple® iOS 11 and above

Supported operating systems for tablet/iPad:

  • Android™ OS version 8 and above
  • Apple® iOS 10 and above

NOTE:
  • When a new version of an operating system is released, it may take some time before the Wiser system is fully compatible with that version.

  • Using Schneider Electric applications with an Android phone that has bypassed restrictions, or a jailbroken iPhone, voids all warranties associated with the application.

  • The compatibility of the interfaces with mobile phones/tablets depends on the software version installed on your mobile phone/tablet, and may change with a software upgrade. Due to the large number of mobile phones/tablets available in the market, the compatibility and functionality of your mobile phone/tablet with the app cannot be guaranteed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.