SUG_Wiser_China_WSE-06

Adding a thermostat to the Wiser Multifunction Interface

In the app, use the Multifunction Interface page to add thermostats that are connected to the interface. Then, control these thermostats using the app.
  1. (See A) In the Multifunction Interface page, tap Add.

  2. On the Add page, set the following:
    • Type: (See B) Air Conditioner or Floor Heater (Floor Heater for this example)
    • Brand: (See C) Schneider for this example
    • Model: (See D) TC300 for this example.
  3. (See E) Set the Unit Address of the thermostat.
    TIP: Refer to Thermostat unit addresses explained for more information.
  4. (See F) Tap Test to confirm that the app switches the thermostat On and Off.
The newly added thermostat is listed on the Multifunction Interface page and is added as a device on the Home page. Tap the device to control the thermostat, change the thermostat name and assign the device to a Room.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.