SUG_Wiser_China_WSE-06

Configuring a Wiser Multifunction Interface

The Wiser Multifunction Interface may have one or more air conditioner or floor heater thermostats connected to any of three channels. To interact with a thermostat using the app, set the channel communication parameters and specify the thermostat make, model and Unit Address.

Before configuring a multifunction interface, add the device to the Home using the procedure Adding a device.

This task uses the example of adding a Schneider Electric TC300 floor heater thermostat connected as the first device on Channel 1 of the multifunction interface. The same method can be used to add other connected thermostats.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.