SUG_Wiser_China_WSE-06

General system

Symptom

Possible cause

Solution

When adding a device, the device is rejected or will not join.

The device may not be supported by the Wiser system.

Only use devices listed in Supported Wiser devices.

When triggering a Moment or Automation with multiple devices, one or more Wi-Fi devices fail to respond.

There may be too many Wi-Fi devices for the router to support.

Performance and stability issues may occur when there are more than 10 Wi-Fi devices connected to the router. Try reducing the number of Wi-Fi devices connected to the router.

Can't add a user from another country to a Home.

If the user is from another country, the account details may be located in a different data store to the Home. See Data stores for more information.

Users can create a another account using a country code in the same region as the Home they wish to join.

NOTE: Users cannot access their own Homes with the new account and must log in to the app with their original account details in order to do so.

The Wiser system cannot connect to the internet via the Wi-Fi network router.

The router port settings may not be properly set for system access to the internet.

Check that the following router ports are open:

  • Port 443 8883 1443

  • Port 6667

  • Port 6668

  • Port 6669

  • Port 6608

  • Port 6681

  • Port 6682

IMPORTANT: For cyber-security, check that all unused ports are closed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.