SUG_Wiser_China_WSE-06

Setting programming mode on a Wiser AvatarOn Freelocate

Perform this task before assigning device control operations to a freelocate or creating a Moment using a freelocate.
  1. On the back of the freelocate, short press the Setup/Reset key 3 times.
  2. Observe that the programming LED on the back of the freelocate displays solid green, indicating that the freelocate is in programming mode.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.