SUG_Wiser_China_WSE-06

Wiser AvatarOn Freelocate

Symptom

Possible cause

Solution

The freelocate LED is blinking orange rapidly.

The freelocate battery may be very low or drained.

Press a freelocate button and observe the operation of the assigned device(s).

If the device does not operate, then the freelocate batteries are drained and must be replaced. (See the installation instructions for the freelocate to replace the batteries.)

NOTE: Always replace both batteries even if 1 battery appears to be sufficiently charged.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.