SUG_Wiser_China_WSE-06

Control devices

Wiser Multifunction Interface

Control the environmental conditions in a home or other building by interacting with HVAC and floor heating systems.

NOTE: A compatible thermostat must be connected to the interface to interact with the app. See Compatible thermostats for the Wiser Multifunction Interface.

Instruction Sheet (PDF)

Wiser IR Convertor

Controls split system air-conditioners, televisions, audio systems and other equipment that can be operated by infrared (IR) remote control.

Instruction Sheet (PDF)

Wiser AvatarOn 2K Freelocate

Wiser AvatarOn 4K Freelocate

AvatarOn T 4K Freelocate

Control Wiser devices and Moments/Automations in the Wiser system with a convenient remote controller.

A freelocate can also be used as a remote controller in an E-mode system. (See About E-mode for more information.)

Instruction Sheet (PDF)

Zigbee 4 Key Freelocate

The Wiser AvatarOn T Zigbee Freelocate (the device) is used to control a group of Wiser Zigbee devices after successful commissioning.

Instruction Sheet (PDF)

Zigbee 6 Key Freelocate

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.