SUG_Wiser_China_WSE-06

Device button/key and LED locations

Find the location of buttons, keys and LED indicators on various devices.

Wiser AvatarOn Switch/Curtain Switch/Dimmer

(See A) Setup/Reset button

(See B) Programming indicator

Wiser 1 Gang Micro Module Switch

WARNING
Danger due to electric shock
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

(See A) Setup/Reset button. Press 3 times on the rocker to activate.

(See B) Status LED

Wiser 1 Gang Micro Module Dimmer

WARNING
Danger due to electric shock
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

(See A) Setup/Reset button. Press 3 times on the rocker to activate.

(See B) Status LED

Wiser Multifunction Interface

(See A) Programming (Prog) button

(See B) Clear button

(See C) Network Status LED

(See D) RS485 port LEDs (ports 1, 2 and 3)

Wiser IR Convertor

(See A) Set/Reset (S/R) button

(See B) Network status LED

Wiser AvatarOn Freelocate

(See A) Setup/Reset button

(See B) Programming indicator

Wiser Window/Door Sensor

(See A) Function key

(See B) Status LED (visible on front of master part when flashing or lit)

Wiser Motion Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser Water Leakage Sensor

(See A) Function key

(See B) Status LED (visible on top of sensor when flashing or lit)

Wiser Temperature/Humidity Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser AvatarOn Air Quality Detector

(See A) Setup/Reset (S/R) button

(See B) Status LED

Wiser Gas Detector

(See A) Setup/Reset (S/R) button

(See B) Status LED

Wiser Smoke Detector

(See A) Setup/Reset (S/R) button

(See B) Status LED

Wiser AvatarOn Smart Socket/ Zigbee 5P Switch Socket

(See A) Setup/Reset (S/R) button

(See B) Status LED

Wiser IP Camera Indoor

(See A) Micro SD Card slot

(See B) Status LED

(See C) Reset Button

Wiser Smart Adapter

(See A) Reset button

(See B) Status LED

Zigbee 6 key Freelocate

See (A) Set/Reset button

ZigBee 1G Switch

See (A) Set/Reset button

Zigbee 2G Switch

See (A) Set/Reset button

Zigbee 3G Switch

See (A) Set/Reset button

Zigbee 1G Curtain Switch

See (A) Set/Reset button

Zigbee 2G Curtain Switch

See (A) Set/Reset button

Zigbee 4K Scene Switch

See (A) Set/Reset button

ZigBee 5P switch socket

See (A) Set/Reset button
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.