SUG_Wiser_China_WSE-06

Wiser IR Convertor

Add infrared-controlled appliances such as televisions, split system air conditioners to an IR Convertor and control them using the app.

Before configuring an IR Convertor, add the convertor to the Home using the procedure Adding a device.

IMPORTANT: If you have a brand-new model of TV, split system air conditioners or HiFi system, the IR code sets may not yet be available in the IR Convertor. The code sets in the IR Convertor are updated regularly, but there may be times when a new model appliance cannot be used with the device.

NOTE: This task uses the example of adding a television to the IR Convertor. The same method can be used to add other infrared-controlled appliances such as split system air conditioners and HiFi systems.

  1. In the Home page, or Room page where the IR Convertor is located, tap the device button to open the IR Convertor page.
  2. (See A) Tap an unused IR Convertor channel. (Unused channels have no name displayed against them.)
    NOTE: IR Convertor channels CH6 to CH8 are only for use with the optional IR extenders.
  3. (See B) Choose TV as the device type then tap Continue.
  4. (See C) Select the television brand.

  5. (See D) If you know the television model number, you can tap Manual and select the model from the list to complete the setup. (Skip the remaining steps.)
  6. If you do not know your television model number, or your television model was not listed in Step 5, you will need to discover the code set by operating a series of remote commands. To do this, first check that the television is switched On and you can see the screen.
  7. (See E) Tap a button on the remote control display in the app. (For example, the Vol + button.)
  8. Do one of the following:
    • If the TV responds as expected: (See F) Tap It works and go to Step 9.
    • If the TV does not respond as expected: (See G) Tap Try next and repeat Steps 7 and 8 using the same button.
  9. Repeat Steps 7 and 8 using a different remote button on the app remote control display.
    NOTE: It may take 3 or more buttons before the IR Convertor recognizes the correct code set.

Once the correct code set has been recognized, the IR Convertor downloads the IR code set. The IR Convertor page is then displayed, with the new television added. Tap the button with the TV name to display the remote page and control the television.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.