SUG_Wiser_China_WSE-06

Wiser system limits

When commissioning a Wiser system, it is important to understand the system limits, such as the maximum number of supported devices. For best performance, it is required to run the system at 80%.

System component

Wiser Hub Limits

Basic Hub Limits

Devices

Max. 120 devices in one Home

Max. 30 devices in one Home

Max. 120 devices in one Room

Max. 30 devices in one Room

Max. 20 devices assigned to a freelocate button

Max. 20 devices assigned to a freelocate button

Max. 10 battery-powered devices per mains-powered device.

Wiser Multifunction Interface

Max. 3 channels per device

Not Supported for Basic Hub

Max. 8 thermostats or controllers per channel

Not Supported for Basic Hub

Wiser 360Degree ZB/IR Convertor

Max. 8 channels (1 IR-controlled appliance per channel)

NOTE: Channels 6 to 8 are reserved for IR extender connections EXT1, EXT2 and EXT3.
Not Supported for Basic Hub

Moments/Automations

Max. 80 Moments in one Home

Max. 80 Moments in one Home

Max. 80 Automations in one Home

Max. 80 Automations in one Home

Max. 80 Actions in one Moment/Automation

Max. 80 Actions in one Moment/Automation

Max. 1000 Actions in one home
(the total actions in Moments and Automations must not exceed 1000)

 
 
 

Max. 10 Conditions in one Automation

Device Schedules

Max. 10 Schedules per device

Homes, Rooms and Members

20 is the recommended number for home per account.

Max. 20 Homes (recommended number)

The installer will be Home owner until successful handover.

Max. 20 Rooms in one Home (recommended number)

Max. 20 Members in one Home (recommended number)

 
 

For information about the recommended distance between the Hub, devices, and sensors, see Selecting a location for the Wiser Hub or Basic Hub . The distance between Hub and device, device and device, and device and sensor is dependent on construction materials or interference in between, it could be a much longer range, in open air, without any interference.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.