SUG_Wiser_China_WSE-06

LED Behavior

Device

Status

LED indication

Duration

Wiser Hub

Switching On/Restarting

All 3 LEDs display solid white

40 s approx.

NOTE: When the device is out of the box for the first time, due to firmware upgrade, the process might take longer than usual (90 seconds).

Connected to router (Wi-Fi)

WLAN LED displays solid white

While connected to router

AP mode commissioning

WLAN LED flashes white.

3 minutes approx.

Level 1 reset in progress

Ethernet/WLAN LEDs flash white

Once

Level 2 reset in progress

Ethernet/WLAN LEDs flash white

3 times

Zigbee network initialized

Zigbee network LED displays solid white

While Zigbee network is available

Zigbee network is Open

Zigbee network LED flashes white

While Zigbee network is Open

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.