SUG_Wiser_Denmark_WSE-09

Safety Information

Important Information

Read these instructions carefully and look at the equipment to become familiar with the device before trying to install, operate, service, or maintain it. The following special messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.

The addition of either symbol to a “Danger” or “Warning” safety label indicates that an electrical hazard exists which will result in personal injury if the instructions are not followed.

This is the safety alert symbol. It is used to alert you to potential personal injury hazards. Obey all safety messages that accompany this symbol to avoid possible injury or death.


FARE
DANGER indicates a hazardous situation which, if not avoided, will result in death or serious injury.
Personer vil komme i livsfare eller alvorligt til skade, hvis disse instrukser ikke overholdes.
ADVARSEL
WARNING indicates a hazardous situation which, if not avoided, could result in death or serious injury.
FORSIGTIG
CAUTION indicates a hazardous situation which, if not avoided, could result in minor or moderate injury.
BEMÆRK
NOTICE is used to address practices not related to physical injury.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.