Abandon Autoupdaters

The following autoupdaters are used by the Abandon tool. They are assigned in the ArcFM Properties Manager on the Abandon Info tab in the On Abandon field.

Component

Description

Used by Feature Classes

Model Names Used

Other Requirements

Product Compatibility

ArcFM Abandon Unrelate and Relate

Unrelates the ConductorInfo table from the conductor before it is abandoned and re-relates it to the conductor after it has been abandoned.

Conductors, Abandoned conductors, ConductorInfo table

MMABANDONRELATE

Details about configuring this autoupdater are available on the Relate/Unrelate ConductorInfo Table page. Refer to this documentation if you wish to configure this AU.

Desktop

Server

ArcFM Change AbandonIndicator field

Changes the value of the Abandon Indicator field to Yes. Abandon Indicator field must have the field model name MMAbandonIndicator assigned.

Abandoned feature classes

MMABANDONINDICATOR (FMN)

Details about configuring to use the AbandonIndicator field are available on the Indicator Field page.

Desktop

Server

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?