Designer Field Model Names
Model Name |
Attribute |
---|---|
DESIGNID |
DesignID attribute in all Feature Classes |
WORKFLOWSTATUS |
WorkFlowStatus attribute in all Feature Classes |
WORKFUNCTION |
WorkFunction attribute in all Feature Classes |
WORKLOCATIONID |
WorkLocationID attribute in all Feature Classes |
WORKREQUESTID |
WorkRequestID attribute in all Feature Classes |
Designer Non-Creatable Features |
|
Model Name |
Object |
DESIGN |
The Design Feature class in the Designer Dataset; prevents this feature class from displaying in the CU tab. |
WORKLOCATION |
The WorkLocation Feature class in the Designer Dataset; prevents this feature class from displaying in the CU tab. |
WORKREQUEST |
The WorkRequest Feature class in the Designer Dataset; prevents this feature class from displaying in the CU tab. |