Rack
This object is required in order to add a PatchPanel to a PatchLocation. This object describes the thing that the patch panel is mounted to or sitting on. Examples include Racks, Frames, Cabinets and Shelves.
Attributes:
Field Name |
Field Type |
Required field? |
Description |
---|---|---|---|
Name |
text |
No |
This is the unique name that the organization gives to the rack. A field that contains a unique name is required by Connection Manager. If an organization does not name its racks and does not have unique names, the ObjectID field for racks can be configured as the unique name through model names. |
RackType |
text |
No |
This field stores the type of structure that holds patch panels and equipment, such as racks, frames, cabinets and shelves. The Fiber Patch Panel Rack Type domain is assigned to this field. |
InstallationType |
text |
No |
This field specifies the location of the rack. It gives an indication as to whether this rack is wall mounted or not. There is no specific functionality tied to this field, so it can be deleted or the number of domain values expanded, depending on the needs of the organization. The Fiber Patch Panel Rack Installation domain is assigned to this field. |
LocationType |
text |
No |
This is a domain-driven field for describing the location of the splice. This can be as specific or broad as needed, but it should cover all possible examples of location types for an organization. The Fiber Patch Panel Rack Location domain is assigned to this field. |
AvailableUnits |
long integer |
No |
This field can be used to store the number of unit values that are available within a rack or frame. IMPORTANT:
|
AvailableUnitsUpdateDate |
date |
No |
This is the date that the AvailableUnits field was last updated. This helps a user determine the currency of the information. |
GlobalID |
GlobalID |
Yes |
This field contains a unique number (GUID) that is generated and maintained by ArcGIS. This value is used for all relationships in the ArcFM data model and is required for Fiber Manager to function properly. |
FiberParent |
GUID |
Yes |
This field contains the GlobalID of the parent object to the current object. |
ThisFiberClassModelName |
text |
Yes |
This field stores the class model name assigned to the feature class on which the field resides. It is used in conjunction with the FiberParentClassModelName field to determine the GlobalID that will be placed in the FiberParent field. |
FiberParentClassModelName |
text |
Yes |
This field stores the class model name assigned to the feature class that is the parent of the class on which the field resides. It is used in conjunction with the ThisFiberClassModelName field to determine the GlobalID that will be placed in the FiberParent field. |
FiberChildClassModelName |
text |
Yes |
This field stores the class model name of a child object to the object on which the field resides. |
-
CreationUser
-
CreationDate
-
LastUser
-
DateModified