TownBorderStation
A town border station is where the gas transmission system is converted to the distribution system.
This feature class has previously used the TBS model name for gas tracing. The TBS model name is no longer used but is supported for backward compatibility.
TownBorderStation inherits attributes from GasStation andGasDevice abstract classes.
Subtypes: None
Associations: Meter
Model Names: TBS
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
PipelineOperatorNumber |
text |
Code indicating pipeline operator. |
Supplier |
text |
Code indicating wholesaler from which gas is purchased. |
EmerIsolationSysHighObjectID |
long integer |
Code indicating the emergency isolation system high side. |
EmerIsolationSysLowObjectID |
long integer |
Code indicating the emergency isolation system low side. |
GasPressureSystemHighObjectID |
long integer |
Code indicating the gas pressure system high side. |
GasPressureSystemLowObjectID |
long integer |
Code indicating the gas pressure system low side. |
GasSystemHighObjectID |
long integer |
Code indicating the gas system high side. |
GasSystemLowObjectID |
long integer |
Code indicating the gas system low side. |