AbandonedGasPipe

The AbandonedGasPipe feature represents gas pipe that have been abandoned in place or used as a conduit; it may also contain selected attributes of GasPipe.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User and designer comments.

ConduitIndicator

text

Represents pipe that can act as casing for a new pipe; domain values include Yes and No.

ConduitLength

text

Length of conduit.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

text

Date of installation.

PropertyUnitCode

text

Value assigned to assets to track and classify property records.

Reason

text

Code indicating reason for casing; domain values include Highway, Railroad, and Street.

RetiredDate

date

The date the device was identified as abandoned.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?