PatchLocation

A patchlocation represents a place where fiber optic service is delivered. These locations are modeled as junction features (single point feature) on the geometric network. These locations have one or more patch panels as well as one or more devices. These features are distinct from DeviceLocations in that they are typically more complex and will always have at least one patch panel.

Attributes:

Field Name

Field Type

Required field?

Description

Name

text

No

This field stores a unique name for the patch location.

GlobalID

GlobalID

Yes

This field contains a unique number (GUID) that is generated and maintained by ArcGIS. This value is used for all relationships in the ArcFM data model and is required for Fiber Manager to function properly.

FiberParent

GUID

Yes

This field contains the GlobalID of the parent object to the current object.

ThisFiberClassModelName

text

Yes

This field stores the class model name assigned to the feature class on which the field resides. It is used in conjunction with the FiberParentClassModelName field to determine the GlobalID that will be placed in the FiberParent field.

FiberParentClassModelName

text

Yes

This field stores the class model name assigned to the feature class that is the parent of the class on which the field resides. It is used in conjunction with the ThisFiberClassModelName field to determine the GlobalID that will be placed in the FiberParent field.

FiberChildClassModelName

text

Yes

This field stores the class model name of a child object to the object on which the field resides.

Common Fields:

  • LocationDescription

  • Owner

  • Comments

  • SymbolRotation

  • CreationUser

  • CreationDate

  • LastUser

  • DateModified

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?