GasMeter
Accurate measurement of volume of gas flowing in pipelines is crucial to well analysis and loss prevention. Meter types include diaphragm, orifice, and rotary.
Subtypes: None
Associations: MeterSetting, RuralTap, TownBorderStation
Model Names: None
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
Comments |
text |
User or designer comments. |
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
FlowCapacity |
text |
Rated capacity in cubic feet per minute (cfm). |
MeterMAOP |
double |
Maximum allowable operating pressure of meter. |
MeterSettingObjectID |
long integer |
ObjectID of associated MeterSetting. |
MeterType |
text |
Code indicating meter type; domain values include Diaphragm, Orifice, and Rotary. |
Owner |
text |
Owner of Meter. |
PressureRating |
text |
Pressure across meter in psi. |
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |
RecordingMethod |
text |
Time recording method to calculate volume. |
RuralTapObjectID |
long integer |
ObjectID of associated RuralTap. |
SerialNumber |
text |
Serial number of meter. |
TBSObjectID |
long integer |
Object ID of associated town border station. |