Data Considerations

ArcFM Electric Tracing relies exclusively upon Feeder Manager’s MMElectricTraceWeight to determine the following essential elements of the circuit connectivity model:

  • Device type of each junction (switching device, transformer, or none)

  • Normal status for each electrical phase of a switching device

  • Transformer phase designation

  • Conductor phase designation

The Bitgate section of the Appendix offers detailed information about how the above data is encoded in the MMElectricTraceWeight integer, and about how a weight autoupdater is used to maintain MMElectricTraceWeight values automatically.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?