Riser

A Riser is a cylindrical or channel enclosure attached to a pole or structure to provide protection for underground conduit as it transitions from overhead to underground. The physical connection between the overhead and underground connection occurs at a pothead.

The Riser class inherits attributes from the Structure abstract class.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

ConstructionType

text

Code indicating construction type of Riser; domain values include 1 Phase Pothead, 3 Phase Riser with Fiberglass Arms, etc.

Height

text

Mounting height of riser on SupportStructure.

Material

text

Code indicating material of riser; domain values include Fiberglass, PVC, etc.

SymbolRotation

double

Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task and ArcFM Auto Angle Setter autoupdater both use this field to rotate point features.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?