How Gas Tracing Works

ArcFM Gas Trace Solvers provide a way to display the results of a variety of traces on the map or as the selected set. For example, you can find all the valves that need to be closed to stop gas flow to an area defined by the user-placed edge flag. Because these queries may be crucial to a utility’s routine maintenance and emergency procedures, this chapter explicitly links the decisions made by the administrator when configuring network features to what the user can expect to happen when traces are performed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?