AntennaDish
This object represents the individual microwave dishes that are attached to an antenna structure or tower.
Attributes:
|
Field Name |
Field Type |
Required field? |
Description |
|---|---|---|---|
|
DishID |
text |
No |
This field contains a unique name assigned to a dish. |
|
DishOwner |
text |
No |
This field contains the owner of the dish. It uses the Fiber Dish Owner domain. |
|
TowerID |
text |
No |
This field contains a unique name assigned to the tower to which the dish is attached. |
|
DishManufacturer |
text |
No |
This field contains the name of the dish manufacturer. It uses the Fiber Dish Manufacturer domain. |
|
DishSize |
text |
No |
This field contains the diameter of the dish and is represented as inches in the US. It may be represented as centimeters in most other countries. |
|
DishType |
text |
No |
This field contains the style of dish. It uses the Fiber Dish Type domain. |
|
Azimuth |
long integer |
No |
This field contains the direction in which the dish is pointed. This value is expressed in degrees. It can be used to determine the microwave path between two antenna dishes on separate towers. |
|
CallSign |
text |
No |
This field holds a value that uniquely identifies the antenna, which is registered with the Federal Communications Commission (FCC) in the US. |
|
Frequency |
long integer |
No |
This field stores the wavelength broadcast and received by the microwave dish. |
|
CircuitName |
text |
No |
This is the name of the fiber optic circuit that this dish completes via a microwave link. |
|
DishHeightAboveBase |
long integer |
No |
This field contains the height (usually represented in feet in the US; meters in other locations) at which the antenna is installed as measured from the base of the tower. |
|
GlobalID |
GlobalID |
Yes |
This field contains a unique number (GUID) that is generated and maintained by ArcGIS. This value is used for all relationships in the ArcFM data model and is required for Fiber Manager to function properly. |
|
FiberOpticCableGlobalID |
GUID |
Yes |
This field contains the GlobalID for the FiberOpticCable. |
|
TowerPointGlobalID |
GUID |
Yes |
This field contains the GlobalID for the tower on which the antenna resides. |
-
CreationUser
-
CreationDate
-
LastUser
-
DateModified