Regulator
A regulator is a mechanical device used for the controlled reduction of pressure in a gas distribution system.
Subtypes: None
Associations: GasStation, RuralTap
Model Names: None
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
Comments |
text |
User or designer comments. |
FlowEquation |
text |
Equation used for analysis of regulator. |
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
Manufacturer |
text |
Code indicating manufacturer of regulator; domain values include American, Fisher, Reliance, etc. |
OrificeDiameter |
text |
Size of orifice. |
Owner |
text |
Owner of associated facility. |
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |
RegulatorStationObjectID |
long integer |
ObjectID of associated regulator station. |
RuralTapObjectID |
long integer |
ObjectID of associated RuralTap. |
SetPressureEntered |
double |
Pressure at which regulator releases to prevent overpressuring within system. |
SetPressureStandard |
double |
Pressure at which the valve is set to release in system standard units, generally psi. |
SetPressureUnitOfMeasure |
text |
Units in which pressure is measured within system. |
SpringRange |
text |
Indicates the number of units over which the spring on the regulator operates. |
TBSObjectID |
long integer |
ObjectID of associated town border station. |