ElectronicMarker

This baseball-shaped device is used to locate a buried fiber optic cable. An Electronic Marker is placed into the trench long with a cable just before both are covered with fill.

Attributes:

Field Name

Field Type

Required field?

Description

MarkerType

text

No

This field specifies the type of markers that an organization deploys in the field. It uses the Marker Type domain.

MarkerManufacturer

text

No

This field describes the company that builds the electronic markers.

MarkerColorFrequency

text

No

This field describes the color of the electronic marker and its corresponding frequency. Typically a red marker will have one frequency, while a green marker will have another. The Marker/Color Frequency domain is assigned to this field.

GlobalID

GlobalID

Yes

This field contains a unique number (GUID) that is generated and maintained by ArcGIS. This value is used for all relationships in the ArcFM data model and is required for Fiber Manager to function properly.

Common Fields:

  • SymbolRotation

  • CreationUser

  • CreationDate

  • LastUser

  • DateModified

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?