International Data Model
Field Name |
Description |
---|---|
CapacityToGround |
The capacitive reactance to neutral or earth of any line segment (ohms per map unit length). |
ConductorMaterial |
Material of which the conductor is made. |
ConductorSize |
Size of the conductor. |
ConnectionOKIndicator |
Indicates whether a line segment is capable of and ready for connection to a load or other line segment. |
InsulationType |
Insulation type of conductor. |
InsulationVoltage |
Withstand voltage of the conductor's insulation (Volts). |
MaxContinousCurrent |
Continuous current rating of conductor (Amperes). |
NumberConductorPerPhase |
Number of conductors per phase. |
OuterDiameter |
Outer diameter of conductor. |
OutOfOrderIndicator |
Indicates whether a line segment is de-energized (for example, out of service for maintenance). |
RatedCurrent |
Continuous current rating of conductor, including any de-rating required for special conditions (Amperes). |
Reactance |
Positive sequence reactance of conductor (ohms per map unit length). |
Resistance |
Positive sequence resistance of conductor (ohms per map unit length). |