MeterSetting
MeterSetting represents the geographical location of a meter or bank of meters at service points. Meters measure the volume of gas flow, which is defined by temperature and pressure.
Assign the LOCATABLEOBJECT model name to enable fields for the Object Query Locator tool.
Subtypes: None
Associations: Meter
Model Names: None
Attributes:
Field Name |
Field Type |
Description |
BypassIndicator |
text |
Code indicating whether meter or meter bank is bypassed; domain values are Yes and No. |
Comments |
text |
User or designer comments. |
FacilityID |
text |
Utility identifier representing a feature's location in the facility; if the feature is replaced, the new feature has the same identifier. Assign the LOCATABLEFIELD model name to enable fields for the Object Query Locator tool. The feature or object class must have the model name LOCATABLEOBJECT assigned. |
GasTraceWeight |
long integer |
Information used for tracing analysis; stored in a bitgate. To support Gas Tracing and Feeder Manager, the model name GASTRACEWEIGHT is required for every feature class belonging to ArcFM gas networks. |
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
InstallationDate |
date |
Date of installation. |
LocationDescription |
text |
Verbal description of location of MeterSetting. |
LocationID |
text |
Utility-assigned identifier of the MeterSetting. |
Owner |
text |
Owner of GasDevice. |
Premise |
text |
Foreign key linking to customer information system. |
SymbolRotation |
double |
Angle that dictates how the feature appears on a map. |
Subtype |
long integer |
Code indicating type of GasDevice, examples include Gas Lamp, Relief Valve, and Gas Station. |