Drip

A drip collects and pumps water that has accumulated in the gas distribution system. Drips are generally installed in low-lying areas.

Subtypes: None

Associations: GasPipe (does not apply to Service)

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

DistributionMainObjectID

long integer

ObjectID of associated Distribution Main.

GasTraceWeight

long integer

Information used for tracing analysis; stored in a bitgate.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

Inspector

text

Name of inspector during last inspection.

InstallationDate

date

Date of installation.

LastPumpedDate

date

Date the drip was last pumped.

LocationDescription

text

Verbal description of location of drip.

Owner

text

Owner of GasPipe.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

SymbolRotation

double

Angle that dictates how the feature appears on a map.

SubType

long integer

Code indicating type of GasDevice, examples include Gas Lamp, Relief Valve, and Gas Station.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?