AbandonedRemovedGasDevice

The AbandonedRemovedGasPipe object represents GasPipe that has been removed; it may also contain selected attributes of GasPipe.

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

PropertyUnitCode

text

Value assigned to assets to track and classify property records.

Reason

text

Reason pipe was abandoned.

RetiredDate

date

The date the device was identified as abandoned.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?