GasDevice

GasDevice is an abstract class. Gas devices control the flow of gas through a network of pipes, measuring and controlling the pressure at which gas is delivered. Features, including GasValve, PressureMonitoringDevice, GasLamp, ReliefValve, GasStation, and RuralTap inherit common characteristics from the GasDevice abstract class.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

EquipmentID

text

Utility-assigned identifier that remains with equipment if it is moved.

FacilityID

text

Utility identifier representing a feature’s location in the facility; if the feature is replaced, the new feature has the same identifier.

GasTraceWeight

long integer

Information used for tracing analysis; stored in a bitgate.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InServiceDate

date

Date device was installed.

InstallationDate

date

Date of installation.

Owner

text

Owner of GasDevice.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

Subtype

long integer

Code indicating type of GasDevice, examples include Gas Lamp, Relief Valve, and Gas Station.

SymbolRotation

double

Angle that dictates how the feature appears on a map.

WorkOrderID

text

Utility-assigned identifier of work order.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?