Circuit Source
A circuit (feeder) is the aggregate of the conductors and equipment downstream of a substation breaker or recloser. CircuitSource stores attributes that describe characteristics of the circuit measured or estimated at the breaker or recloser. These attributes include capacity, measured in kilowatts (kW); resistance, measured in ohms; and load, measured in reactive kilovolt-amperes (kVAR).
Associations: BusBar, CircuitBreaker, Recloser
Subtypes: kW, Swing, Voltage Controlled. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.
Model Names: CIRCUITSOURCE
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
BusBarObjectID |
long integer |
ObjectID of associated BusBar. |
ConnectionConfiguration |
text |
Code indicating configuration of conductors; domain values include Delta, Wye, etc. |
DynamicProtectiveDevObjectID |
long integer |
ObjectID of associated dynamic protective device. |
EmergencyCapacitykW |
long integer |
Emergency rating of CircuitSource, in KW; domain values include 12. |
FeederSourceInfo |
long integer |
Stores information about source of feeder. Feeder Manager requires the FEEDERSOURCEINFO model name on this field. Feeder Manager uses this field to determine whether a feeder has features that participate either loop or multifeed situations. |
GroundReactance |
double |
Reactance of ground seen at the source by the downstream circuit. |
GroundResistence |
double |
Resistance of ground seen at the source by the downstream circuit. |
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
ID |
text |
System-generated identifier of feeder initiated at this source. Feeder Manager uses the FEEDERID model name on this field. |
MaximumCapacitykW |
long integer |
Maximum allowable operating capacity of CircuitSource; domain values include 10. |
MaxKVAR |
long integer |
Maximum kVAR load experienced at CircuitSource; domain values include 6. |
MaxPositiveSequenceReactance |
double |
Maximum positive sequence reactance seen at the source by the downstream circuit in ohms. |
MaxPositiveSequenceResistance |
double |
Maximum positive sequence resistance seen at the source by the downstream circuit in ohms. |
MaxZeroSequenceReactance |
double |
Maximum zero sequence reactance seen at the source by the downstream circuit in ohms. |
MaxZeroSequenceResistance |
double |
Maximum zero sequence resistance seen at the source by the downstream circuit in ohms. |
MinFaultCurrentOH |
long integer |
Calculated minimum fault current for overhead conductors. |
MinFaultCurrentUG |
long integer |
Calculated minimum fault current for underground conductors. |
MinkVAR |
long integer |
Minimum kVAR load experienced at CircuitSource; domain values include 500, etc. |
MinPositiveSequenceReactance |
double |
Minimum positive sequence reactance seen at the source by the downstream circuit in ohms. |
MinPositiveSequenceResistance |
double |
Minimum positive sequence resistance seen at the source by the downstream circuit in ohms. |
MinZeroSequenceReactance |
double |
Minimum zero sequence reactance seen at the source by the downstream circuit in ohms. |
MinZeroSequenceResistance |
double |
Minimum zero sequence resistance seen at the source by the downstream circuit in ohms. |
Name |
text |
Utility name of CircuitSource. Feeder Manager uses the FEEDERNAME model name on this field. |
NominalVoltage |
long integer |
Code indicating system voltage for which CircuitSource is rated; domain values include 7.2 kV Grounded Y, 24.9 kV Grounded Y, 2400 Delta, etc. |
OperatingVoltage |
long integer |
Code indicating standard level of voltage at which system is currently operated in kV; domain values include 12.5 kV Grounded Y, 7.2 kV Grounded Y, etc. |
SubstationID |
text |
Substation identifier. Feeder Manager uses the SUBSTATIONID model name on this field to identify the substation that acts as a source. |
VoltageAngle |
double |
Angle at which phase is offset from system standard. |