Communication Cable

CommunicationCable carries nonelectric signals within the network. Structures, mainly poles, may be used under a joint ownership agreement or lease to support power and communication lines. Other utilities or entities may attach cables that carry signals such as CATV. CommunicationCable can also be used to control SCADA equipment. CommunicationCable inherits the attributes of ElectricComplexEdge.

Conduit Manager uses the ULSMEMBER model name to designate the CommunicationCable feature class as an edge that can be found within a conduit.

Associations: None

Subtypes: None

Model Names: ULSMEMBER

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?