PipeLineMarker

A pipe line marker is placed as closely as practical over an underground gas line to identify the location of the facility and reduce the possibility of damage or interference.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Condition

text

Physical condition of PipeLineMarker.

Comments

text

User or designer comments.

DateInspected

date

Date of last inspection.

DimensionTie1

text

Description of east–west line of feature location.

DimensionTie2

text

Description of north–south line of feature location.

EquipmentID

text

Utility identifier that stays with equipment if it is moved.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InServiceDate

date

Date PipeLineMarker was set in service.

Installation Date

date

Date of installation.

NextInspectionDate

date

Date of next inspection.

Owner

text

Owner of PipeLineMarker.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

SymbolRotation

double

Angle that dictates how the feature appears on a map.

WorkOrderID

text

Utility-defined identifier of work order.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?