Demand Info

Demand from the customer is the load at receiving terminals averaged over a specific time. Industrial and commercial customers can be billed for having sufficient power available. This demand charge is measured in kVA and is over and above the charge for kWh. A power factor charge may also be billed to large customers to offset the necessity of having to provide reactive power to serve large motor loads.

Associations: None

Subtypes: None

Model Names: DEMANDINFO

Attributes:

Field Name

Field Type

Description

kW

long integer

Load demand in kilowatts.

kVAR

long integer

Reactance in reactive volt-amperes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?