Domain Independent Field Model Names

Model Name

Object

AMPS

Assign to any field that represents the amperage of a rectifier feature class that participates in the cathodic protection system of a gas or water network.

DESCRIPTION

Assign to any field that is the description of a feature. Be sure to assign this model name to rectifier, anode, and test point feature classes that participate in the cathodic protection systems of gas and water networks.

INSERVICEDATE

Assign to any field that represents the Inservice date of a rectifier, anode, and test point feature class that participates in the cathodic protection system of a gas or water network.

INSETFRAMETITLE

Assign to any field that is the title of inset frame windows.

INSETFRAMESCALE

Inset frames are scaled by the value in the field to which this field model name is applied.

INSETFRAMESORTINDEX

Inset frames are sorted by the field to which this field model name is applied.

LABELTEXT

The attribute on the conductor feature class that stores information about related ConductorInfo objects. Used by the ArcFM Update Primary Conductor Text special AU and the ArcFM Update Conductor Text relationship AU.

LOCATABLEFIELD

Assign the LOCATABLEFIELD field model name to enable fields for the Object Query Locator tool. The feature or object class must have the model name LocatableObject assigned.

MAPGRIDNAME

The attribute on the ArcFM Map Grid feature class that stores the name of the grid; used for Map Grid Generator tool.

MAPSHEETANGLE

The attribute on the ArcFM Map Grid feature class that stores the angle of the map sheet; used for Map Grid Generator tool.

MAPSHEETNAME

The attribute on the ArcFM Map Grid feature class that stores the name of the map sheet; used for Map Grid Generator tool.

MEASUREDLENGTH

Assign to measured length field

MMABANDONINDICATOR

The attribute on any feature class that indicates whether or not a feature has been abandoned.

MMCONDUITINDICATOR

The attribute on any feature class that indicates whether or not the feature has been converted to conduit.

PATH

Assign to file path field of map inset tool.

QAEXPORT

Assign to any field that should be exported to a file or report using the QA/QC tool.

SERVEROID

The attribute that is used to store the ObjectID of the feature class.

SYMBOLROTATION

This model name is assigned to a field on point feature classes that indicates the angle by which the feature is rotated when it is placed on the map.

VOLTS

Assign to any field that represents the voltage of a rectifier feature class that participates in the cathodic protection system of a gas or water network.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?