Reclose Sequence

This object is required to enable the Network Adapter CIM export to DMS.

Associations: DynamicProtectiveDevice (only valid for subtype Recloser)

Subtypes: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Step

short integer

The ordinal position of the reclose step relative to other steps in the sequence.

Delay

double integer

The time lapse before the reclose step will execute the reclose.

FastType

long integer

True if the reclosing step is fast; otherwise, false.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?